Moja osoba do kontaktu
igus® Sp. z o.o.

ul. Działkowa 121C

02-234 Warszawa

+48 22 863 57 70
+48 22 863 61 69

Automatic cutting machine

This application is intended to be used as a safety function on an automatic cutting machine, which stops the machine if the yellow paddles meet an obstacle. Before the use of the igubal® spherical bearing, the machine used a process in which pressure was applied. A drop in pressure stopped the machine.

The spherical bearing compensates the angle misalignment. That means no more maintenance is necessary.

Automatic cutting machine

Go to applied products here

Further interesting applications from extremely diverse areas can be found here.

Go to manus® contest