Zmień język :

Silnik jest zasilany energią za pośrednictwem kabla silnikowego, który zawiera żyły — trzy czarne dla faz L1, L2 i L3 oraz zielony i żółty dla żyły uziemiającej. Obecnie uzwojenia cewek w silniku są zwykle połączone w gwiazdę lub trójkąt. W ten sposób liczba żył jest ograniczona do czterech. Można wybrać kabel z ekranowaniem lub bez, w zależności od wymagań kabla w odniesieniu do zakłóceń lub wrażliwości środowiska. Oczywiście kable są produkowane z różnymi rodzajami płaszcza i klasami mechanicznymi.

Why motor cables?
When professionals talk about motor power, they usually don't just mean a supply cable for a motor. A four-core control cable can also represent this. The point is that you want to connect the motor to a frequency converter (FI). The prerequisite for this is that the insulation of the core fulfils the voltage level of 600/1000V. This is necessary because the frequency converter uses the principle of pulse width modulation to regulate the frequency and therefore the motor speed. This leads to voltage peaks, which the insulation must be able to withstand. For this reason, a higher voltage class is selected than that of a control cable.

Multi-core vs. single core
For large drives in particular, it is now common to run the cable in single cores. This solution offers several advantages over the classic four-wire multi-core. The biggest advantage is probably the significantly lower price, which is achieved through a different, cost-effective manufacturing process. The single-core solution is also robust and therefore suitable for small installation spaces in the energy chain, while at the same time offering a longer service life. This is particularly noticeable on long travels. The connection to the motor is easier with the thinner single-core cables, but requires a special screw connection. We are very experienced with challenges of this kind and therefore always have the required products for the solution in stock.
Advantage of TPE for abrasion, cold and service life
The majority of our motor cables have the high-end material TPE as the outer jacket material. This material is particularly suitable for applications in extreme temperature ranges. This is because the temperature range for TPE motor cables is defined in energy chain as -35°C to +90°C. This means that applications in deep-freeze areas or applications in very warm environments are just right for this material. In addition, TPE has another special feature - maximum abrasion resistance. In direct comparison to PVC & PUR, TPE has better abrasion behaviour and is therefore ideal for high-end applications for the highest service life.

Motor cables in crane systems
igus has been equipping crane systems with energy chains for many years. Well over 10,000 crane systems are in long-term use worldwide. The cable and chain withstand the most adverse conditions, from -40°C in the Siberian winter to 50°C in the harbour of Dubai. A cable failure is unimaginable in crane and trolley operations. Maximum reliability is required in these areas. This is why, for example, single cores from the CF330.D or CF340 series are used throughout to supply the hoist with nominal conductor cross-sections of up to 185mm. This can be seen as a development towards standardisation. The next time we plan an application with a large cross section, we should definitely discuss a concept with single cores that have a high-quality braided conductor.
Łatwe wyszukiwanie, wybór odpowiedniego typu, obliczanie żywotności i zamawianie online

Wyszukiwarka produktów
Szybkie wyszukiwanie odpowiedniego kabla

Kalkulator żywotności
Obliczanie żywotność dowolnego przewodu chainflex

Kalkulator dodatku miedziowego
Obliczanie dziennego dodatku miedziowego

Konfigurator niestandardowych kabli
Skonfiguruj swój niestandardowy kabel w zaledwie 3 minuty



Osobista:
Od poniedziałku do piątku: 7:00–20:00
Sobota: 8:00–12:00
Online:
Umów spotkanie z ekspertem